Cables and Wires - Ready for China

Certified products for export

We are “Ready for China” - Are you?

HELUKABEL® has been represented in China for more than 12 years and has a wide product program specially developed for the Chinese market. HELUKABEL® China addressed the challenges of the CCC certification (CCC = China Compulsory Certification) at an early stage and provides the largest assortment of cables and wires with the "Ready for China" rating. This makes it possible for us to simplify the complexity of the Chinese certification, which requires significant personnel and financial effort. Talk to us, we would be glad to advise you!

HELUKABEL® China – 4 locations for maximum coverage

With 4 locations, HELUKABEL® is represented in the most important economic regions along the east coast. This includes the so-called Pearl River delta in the Guangdong province with the special economic zone Shenzhen, Shanghai located in the Yangtze delta as well as the metropolitan area of Beijing. This is where more than 30 expert consultants are available for you with advice, of course also in German and English.

In Taicang, HELUKABEL® produces cables and wires for the Asian market from a 7,000 m² manufacturing facility. Similar to the plants in Germany, the focus is on high quality, flexible and highly-flexible cables and wires, which are produced in accordance with German, Chinese and international standards and norms. Flexible production cells permit short delivery times.

Based on a comprehensive stock program at different locations, cables, wires and accessories can be called up directly at the location without any time delay. The new HELUKABEL® logistics centre in Taicang is also used as a product hub for the entire Asian market and offers significant benefits especially for the processing of large projects that are critical with respect to time and volume. At the same time, we frequently ship by air and sea freight from Germany. More than 70 cable types, have been documented and approved for a quick and easy movement of goods.