Production in Germany

Cable manufacturing plants in Windsbach and Meissen

In our two facilities we manufacture according to the latest production methods, and annually we produce approx. 1 million conductor kilometers (that’s 77 times around the globe!). More than 300 employees are specialized in making high-quality standard and specialty cables.

 Using the latest in cable technology material, and cooperating with international testing institutes, makes us an innovation leader in the areas of automation, data technology, building management systems, and renewable energy.

Production figures:

  • 40 000 m² production facility
  • 25 extruder facilities
  • 20 stranding machines
  • 50 braiding machines
  • Cables & wires from 0,05 to 1000 mm²
  • According to: EAC, UL-CSA, HAR, CCC, Germanischer Lloyd, TÜV or according to customer specifications

Production extension at Windsbach plant

The actual construction of a further building complex, aims to concentrate the worlds research and development capacities in Windsbach as well as to establish the test facilities in the new technology centre.

Once the construction has been completed in autumn 2016 the new offices, laboratories and production areas will have a capacity of 9000 m². The investment of 20 million Euro is a clear commitment to the location of Windsbach.